Eaton Logo

Are special tools required to use SmartWire-DT?

There are two special crimping tools required for the SmartWire-DT flat cable. One is used to crimp the flat plugs at each end of the cable (SWD4-CRP-2) and the other is used to crimp the device plugs along the cable (SWD4-CRP-1).