Eaton Logo

How are the powerfeed modules in the SmartWire-DT system applied?

The SmartWire-DT powerfeed modules are put in line with other components in the SmartWire-DT network. They are used for
different tasks; module 1 is used to add extra 24Vdc power to provide additional power to multiple contactors with large draws.
Module 2 is used to accomplish the same task as module 1 however; it also adds the 15Vdc power needed by the SmartWire-DT network to support large connection bases, or large runs of the SmartWire-DT network.