Eaton Logo

What space requirements are necessary to include SmartWire-DT in an existing panel?

When converting or adding SmartWire-DT to a panel, space is required for the modules that connect to the top of the contactors, roughly 1” (25mm). The SmartWire-DT gateway and powerfeed modules require 1-3/8” width of DIN rail.