Eaton Logo

How is device addressing done on the SmartWire-DT network?

SmartWire-DT assigns node addresses automatically when the auto-config button on the gateway is invoked. There are no DIP switches to be set on the modules nor do modules have to be programmed separately. SmartWire-DT makes it easy to connect. If a module has to be replaced, the auto-config addressing process with find and address the new node without any reprogramming.