Eaton Logo

How do I add images and graphics to a screen in HMiSoft?

Please see the instructions below and let us know if you have any questions:

1) Open up a project, go to 'Options' at the top, and select 'Picture Bank'

2) Click the folder icon with the green arrow (top left of the window), type in a name for the Picture Bank, click 'OK', and exit the window

3) An easy way to add an image is to place it within a rectangle. Right click on the screen, scroll down to 'Drawing', and select 'Rectangle'

4) Select the 'Picture' tab and choose the Picture Bank name that you created earlier. A 'Select Picture' window will pop up where you can import an image into the picture bank. Select the picture after importing it and hit 'OK'. Edit the image properties in the same window and you are done.