Eaton Logo

how to use the SVX drive for the single phase input supply?

Please consider the below points for selecting an SVX drive for single phase application.

1)The motor used at the output of the drive must be three phase.

2) The single-phase input voltage to the drive must be the same magnitude as the three-phase output voltage required by the motor.

3) The FLA of the motor being used is recommended to be used for sizing the VFD, not Hp.

4) The attached Application Note is for Variable Torque applications only. If you have a Constant Torque application, please contact the VFD Quotations group below for assistance choosing the appropriate VFD.

quotationsvfd@yahoo.com or 1-800-322-4986, option 1

 

 

  1. SVX_Single_Phase_App_Note.pdf