How much % line reactor does Eaton offer in the input side of the LV drives?
The Eaton drives (DG1, DH1 and the HMAX) have 5% DC Link Chokes as a standard, that is comparable to a 3% Line Reactor as a whole.
If the requirement is of total 5% line reactor than we need to add the the line reactors externally based on the specifications of the drive.
For making a proper selection of the line reactor please contact Eaton support team at vfdquoations@eaton.com