Eaton Logo

Is the cable that is in DXG-ACC-SOFTWARE the same cable as DXG-CBL-PCCABLE

DXG-CBL-PCCABLE part number is the cable only part number and all software and manuals to connect to the drive can be obtained at www.eaton.com/dg1 under the software tab.

DXG-ACC-SOFTWARE includes the cable, manual, and software on a CD.  It is recommended that you check the rev of firmware/software on the CD against the web link at www.eaton.com/dg1 if possible to ensure there are no firmware compatibility issues.

The PC cable in DXG-ACC-SOFTWARE included is the same cable that the part number DXG-CBL-PCCABLE is associated with.