Eaton Logo

What are the part numbers for the copper straps for Enclosed Control non-fuse controllers?

Enclosed Control Fused Disconnect Shorting Strap Kits that are available are listed below. Before installing the shorting straps be sure that the the branch circuit protection is in place for the load as required by the NEC or AHJ. 

Current                Size        Cat No                  

30AMP:                0, 1         99-2428-6            

60AMP:                2             99-2428-7           

100AMP:              3             99-2428-8         

200AMP:              4             99-2428-9    

 

These will need to be price by the TRC (Technical Resource Center)    

Need a technical support person?