Eaton Logo

What is the reverse voltage present when the DC coil of a XTRE relay is de-energized ?

 The reverse voltage is about 2.5 times higher than the coil voltage, example: 24 V coil voltage = 60 V reverse voltage.