Eaton Logo

What is the frequency range allowed for the XTPE motor protector?

The XTPE can be used for a frequency range of 20Hz to 120Hz and can therefore be used on the load side of VFDs to control smaller HP motors. However, the normal current measurement capability that you have using SmartWire-DT with the XTPE is not recommended when used in this configuration.

What is SmartWire-DT?