Eaton Logo

What is the mode of operation for the trip indicating auxiliary contacts on the XT MMP?

The trip indicating auxiliary contacts do not change their normal NC state when turning the MMP on or off using the handle.  The contacts only change their normal NC state to NO when either a overload or short circuit trip occurs or you if initiate a test using the test button. Click IL03402030Z  which attempts to show the contact state for both overload “+” and short circuit “I>” trips. 

If you need the contacts to change state when either the unit trips or if it is physically turned on or off then I’d suggest the standard aux contacts: