Eaton Logo

What is the Maximum temperature withstanding rating for the terminals of FAZ breaker

The FAZ breakers are suitable for use with 60 or 75°C wire.  If you choose to use 90°C wire you must not use it past the 75°C ampacity for the given wire size