what is the temperature ratings of the BAB/BABH lugs?
Quicklag breakers are UL 489 rated. UL 489 dictates that breakers 100A and under may be used with wire rated 60°C or 75°C. The trip curves for Quicklag breakers all reference using either 60/75°C wire, or 75°C wire for breakers over 100A in current rating. Therefore the terminals, themselves, are 75°C rated.