Eaton Logo

How do I determine characteristics for an ELQ breaker?

ELQ breakers are unique to Eaton Electric Australia. It is a Quicklag combined overload and earth leakage breaker. The breaker characteristics are 30mA/10mA rated tripping current. Symmetrical Interrupting capacity of 6kA of 250VAC. 

There are no equivalents in the domestic or international quicklag breaker line. The closest breakers in the Domestic outfit are the QCGFEP, QBGFEP, QPGFEP which are 10kAIC/22kAIC of 120VAC.