Eaton Logo

How to thermally derate Quicklag Type Breakers?

No derating chart exists for derating Quicklag breakers in the field. The amperage rating is labeled on these breakers, and derating in the field would cause the breaker to be mislabeled. Standard temperature rating is 40C (40 Degrees Celsius). Call the technical resource center at 1-877-386-2273 for availability of factory derating for Quicklag breakers. For 50C calibration, add suffix "V"

CAUTION: Always consult a licensed electrician. Always adhere to local code requirements.