Eaton Logo

What is the replacement for a British Standard Miniature Breaker?

Rated voltage and British standard information must be checked in newer series.  For example, the QC2040HE breaker has the British Standard Marking (E) with a 240/415 VAC rating . The QC2040H is the exact same breaker but does not have the British Standard Marking and is rated at 240VAC.