Eaton Logo

What is the terminal torque values of QCR/QCF breakers?

The terminal torque values are listed on the side of the breakers.  They are:  

4-6 AWG wire use 26 In lbs

8 AWG wire use 25 In lbs

14-10 AWG, use 20 In Ibs.