Eaton Logo

What is the difference between RE and REA circuit breakers?

RE circuit breakers are built with off center terminals on the line side.

Both the RE type and REA type are panelboard replacement circuit breakers. RE circuit breakers are built with off center terminals on the line side. REA circuit breakers are built with terminals on the line side. The two styles are available to accommodate varying panelboard bus arrangements.