Eaton Logo

What are the torque requirements of the G-frame breaker?

Torque requirements are on the breaker nameplate. Amount of torque depends on the size of wire being connected. 14-10 AWG 20 in.-lb.; 8 AWG 40 in.-lb.; 6-4 AWG 45 in.-lb.; 3-1/0 AWG 45 in.-lb.