Is a folding handle extension available for Eaton N-frame molded case circuit breakers?
A folding handle extension is available for Eaton N-frame molded case circuit breakers. The handle folds side-to-side. The handle extension is available for purchase through the standard authorized Eaton Electrical group distribution channel as style number 5114A74G03. From the center of its pivot point where it bolts to the N-frame circuit breaker toggle handle, the folding handle extension is 6.60" long. An image of the N-frame folding handle extension is shown below.