Eaton Logo

DIGIVIEW memory, COT retention, battery expiration

DIGIVIEW is built with no memory, but is built with a backup battery; display of cause-of-trip (COT) information and current flow information is real-time only.  If the circuit breaker upon which DIGIVIEW is installed trips and remains so, and the DIGIVIEW backup battery happens to expire after a period of time (LEDs displaying COT are extinguished), then COT information is lost and is irretrievable.