Eaton Logo

What ground lug should be used with enclosed molded case circuit breakers?

Ground lugs for enclosed molded case breakers are not included when purchased from Eaton. Neutral kits (capable of being bonded to ground) can be purchased separately. These parts are located in the catalog. Separate ground lugs can also be purchased. These parts are listed in the catalog on the accessories page for safety switches. The ground lug size should be selected based on the frame rating of the breaker, or the closest match to the breaker frame rating.