Eaton Logo

Motor Protection

What is the difference between the hot and cold overload curves used by the C440/XTOE overload?

What can cause a phase reversal fault in an S811+?

Do you have a adjustment guide for the overload settings for the C440 / XTOE when using current transformers?

Why is my C440 / XTOE solid state overload status LED continually blinking?

What is a "pass through" overload relay?

How to determine over load trip setting for C440 relay from motor FLA rating ?

D65 Product Overview

How much does Power Xpert inControl Software cost?

C440 Overload Relay Test Procedure

Where can I find documentation for the C441 Motor Insight Relay?

How will inrush current effect the thermal memory of the C440 overload relay

How does the Thermal Memory work on the C440 Overload Relay

Do Eaton low voltage motor control products with 2 Ethernet ports support Device Level Ring (DLR) on Ethernet/IP?

What is the difference between C440 XTOE and ZEB overload relays?

Is the ZEV overload relay still available?

Can I wire my solid state overload relay for a single phase application?

C445 Documentation

Can you use the motor insight C441 or C445 overload relays on the output of the drive/VFD?

Ground fault protection class for the C441 overload relay

Is there a way to disable the phase imbalance during the motor start only for the C440 relays??

What is the longest allowable Ethernet patch cable length?

Using the Power Xpert inControl software, what is the best way to save C445 configuration?

Do you offer Add-on-Instructions for Motor Protection products C440 C441 C445

What components are required for a C445 system?

If the C440/XTOE “phase unbalance” dip switch selector is OFF, is “Phase Loss” protection will be also at OFF?

Can I use Series B heater packs in Series A C306 overload relays?

C440 / XTOE Product Overview

C441 Product Overview

Where can I find documentation for the C440 / XT Electronic Overload Relay?

What is the factory stated accuracy of the XTOE / C440 OL trip tolerance?

Are the CN35 Lighting Contactors ROHS compliant ?

Do I need an overload for the AN19 ?

C440 LED is not flashing

What is fault code 20 indicating on the motor insight C441 motor protection relay?

How is power calculated in motor insight C441 overload relay?

Operation Temperature of CN35 Lighting Contactor

Looking for a Westinghouse Groundgard relay

XT Combinational SCCR Ratings (UL508A)

where can I find replcement for 9441H400 drum switch?

What is the solution to replace C316FNA_ Overloads?

What is a DTM in the Power Xpert inControl software?

How many Ethernet connections (sockets) do the C441 Ethernet modules support?

Can the USB/Micro USB cable (part number: C445XS-USBMICRO) for the C445 Motor Management relay be used to upgrade the firmware on the C445?

What does “rOF” mean on the C441 Motor Insight display?

When using an ABB controller with the C441 PROFIBUS modules, why do I get an error when installing the GSD file for the C441 PROFIBUS modules into the ABB software?

What is the difference between 2-wire and 3-wire fieldwire control for a C445 Motor Management Relay?

When using Modbus serial or Modbus TCP to operate and monitor a C445 Motor Management Relay, can I read scattered Modbus registers with a single read message?

What are the functions of the C440/XTOE Health Status LED?

How do you connect modules in the C445 Motor Management Relay?

How do you connect to C445 using Power Xpert inControl?

How do I set the CT ratio and FLA on a C445 w/ external CT's?

Is C441 available in Enclosed Pump Panels?

What is the FLA adjustability range of a C440?

What does the C445 Setup Wizard do?

Is is possible to upgrade firmware on C445 once installed?

What is the PTC protection feature offered in C445?

Does C445 allow you to set a Communication Loss Timeout value?

Are the phase unbalance and phase loss protection tied together in the C440 relay?

How does D65PLR480 Series, Phase Loss and Reversal relay works

C441 Lower Display Threshold

How do the D65 monitoring relays work?

What do I replace my CEP7 old obsolete solid state overload relay with?

C445 Accessories & Replacement Parts

C445 Selection

How do I select a C441 Motor Insight Relay?

What are the functions of the inputs on the C445 Global Motor Management Relay?

Can the C445 overload protection relay be used in single phase applications?

What type of ground fault is used in the C440 and XTOE solid state overload relay?

How do I select a heater for size 5 or larger starter with CTs?

C445 Drawings

What is the ground fault protection class for XTOE / C440 overload relays

What is a motor management relay?

Are supplementary fuses required for C441 motor insight voltage input terminals

What is the UL file number for C445 motor protection relay

C445 demo stand instructions

What is the UL file number for the C441 motor insight overload relay

What if the UL file number for the IQ500 overload relays?

Is there any way to manually reset the thermal capacity to zero on the C441 motor insight?

What does the error code F20 stands for on C441 Relays

Random rOF Fault on Motor Insight C441

Can I use the aux contacts to shunt trip my breaker using motor insight C441 overload relay

recommended fuse for D64L2 relay test circuit

Can the C440 or XTOE overload relay be used for DC applications?

What is the processor speed of C441U ? How often C441U reads its inputs ?

Do the A200 series thermal overload relays have a DC voltage rating ?

What are the communication capabilities of various motor protection overload C440/C441/C445?

Do you still offer the type FT overloads ?

Does the C445 Motor Management Relay have a Real Time Clock?

My C445 has a fault following disconnecting the optional user interface. What do I do to clear the fault?

How do I get the USB/micro USB cable for the C445 Motor Management Relay to work with the Power Xpert inControl software tool? Where do I find the USB driver?

How do I select the Local and Remote control modes for a C445 Motor Management Relay?

Do I need to change my PLC program if I switch from using Advantage starters on DeviceNet (WPONIDNA) to either C440 or C441 overloads?

What control sources can be used with a C445 Motor Management Relay?

What industrial networks do the Eaton overloads connect to?

Do I need to manually enter all descriptive I/O tags into RSLogix5000 for Eaton Motor Control products?

Do Eaton motor control and protection products connect to Ethernet/IP?

What should a customer do who is experiencing communication issues with C441 Ethernet/IP products or drives on Ethernet/IP?

What is the shortest allowable Ethernet cable length?

How do I save an entire project with the Power Xpert inControl software?

Does the C445 Motor Management Relay support DeviceNet