Eaton Logo

What are Add-On Instructions for the Eaton motor control products on the Eaton website used for?

Add-On Instructions (AOIs) are for Eaton low voltage overloads, drives and soft starters when they are on Ethernet/IP networks with a Rockwell PLC. They import into RSLogix5000/Studio5000 and provide descriptive tags for each I/O tag for specified I/O assembly pairs. They also take care of scaled parameters like motor current and provide them in engineering units and as a Real value to retain resolution. Instructions for importing them into RSLogix5000 and how to implement them are provided in a zip file with each AOI.