Eaton Logo

How do I configure the DIP switches on an Advantage Starter

Positions 5, 4, 3, 2, 1 set the current range (In general as the settings go from 00000 - 11111 the current range increases).

Position 7 and 6 set the overload class:

00 for Overload Class 10

01 for Overload Class 20

10 for Overload Class 30

11 for No Overload Class

Position 8 sets the reset mode:

0 for Manual Reset

1 for Automatic Reset