Eaton Logo

Where do I find renewal parts for the Freedom contactors and starters?

Renewals parts for Freedom contactors and starters can be found in the aftermarket catalog, volume 12, tab 13. Click on the link below and go to table of content and find Freedom.  Note that the 120Vac coil and 208V coil have migrated from the old 9-2703 numbers to the 9-3285.  Either coil will work in any of the Size 1 Freedom contactors.  But the ones being sold today are the 9-3285 versions.  The other coil voltages are still using the 9-2703 #.  

 

Freedom Renewals