Eaton Logo

What is the burden of the digitrip power supply?

  • The power supply for the Magnum digitrip 1150, 520M, and 520MC has a burden of 10 VA.
    • The input voltage ratings are 120VAC, 230VAC, 24-48VDC, and 125VDC.
  • The power supply for the NRX digitrip 1150, 520, and 520M has a burden of 6 VA.
    • The input voltage rating is 24VDC.
  • The power supply for the NRX PXR trip unit (Power Defense) has a burden of 6 VA.
    • The input voltage rating is 24VDC.
  • The power supply for the VCP-T digitrip 1150V, and 520MCV has a burden of 10 VA.
    • The input voltage ratings are 120VAC, 230VAC, and 24–48VDC (125VDC for the 520MCV).