Eaton Logo

PSG Power Supply Selection

The following information is required when selecting a power supply. The current offering is the PSG series which has replaced the PSS type:

  • Nominal Input Voltage (100-240 VAC or 200-500 VAC)
  • Output Voltage (24 or 12 VDC)
  • Nominal Capacity (Watts or output current in Amps)
  • Surge Capacity (Amps)

With this information, individual part numbers can be selected from the catalog: Volume 7, Tab 6 - Power Supplies

Frequently Asked Questions

What kind of power supply do I need for the S801+ /S811+ soft starters?

What power supply output voltages are available?

For more information, see our PSG Power Supplies Product Overview