Eaton Logo

What is the difference between a timer being "power trigger" versus "control switch trigger"?

A control switch trigger timer is going to require a dry contact closure onto the timer to start the timing function and requires control power continuously on the timer. The Power trigger will start once the timer is powered onto the power trigger terminals and will not required a dry contact closure. The power trigger timer will also require control power continuously on the timer.