Eaton Logo

How do the PSG power supply buffer modules work?

The buffer module use maintenance-free electrolytic capacitors to store energy. In the event that the input voltage to the system is lost briefly, the stored energy in the buffer module allows for the load to remain powered for 250ms at 20A or 5s at 1A