Eaton Logo

What is the current surge or outrush current on the PSG power supplies?

All PSG power supplies are capable of providing 1.5 times the nominal current for up to 1 second. The current surge can be repeated every 10 seconds without system shutdown. It is important to note that repeated overloading will reduce the expected life of the unit.