Eaton Logo

Soft Starters

What can cause an SCR failure on a soft starter?

What breaker size do I use for an S811+ soft starter?

Why won't my S811 or S811+ soft starter start?

What can cause a phase reversal fault in an S811+?

S811+/S801+ Shorted SCR

DS7 Phase Failure Fault

What is the S811+ Internal Bypass Contactor Voltage Drop?

What to the Flashing LED's on the S811+ Mean?

How Long does the Soft Starter last? what is their effective useful life?

Do the S801+ and S811+ have communication ability?

How is the Phase Loss protection determine for the S611 soft starter?

What is the new catalog number for an S801N37N3B?

What accessories and replacement parts are available for the S801+ / S811+ Soft Starter?

Do you have a refurbished or exchange program for soft starters?

Is the S811+/S801+ marked with Environmental Friendly Use Period (EFUP) information?

S811+ /S801+ Product Overview

How many starts per hour will the S811+ allow?

Where can I find drawings for the S801+ / S811+ Soft Starter?

Can I replace my wye-delta controller with a soft starter solution?

Frequency operating range for Eaton's S811+ soft starters?

Why can't I clear an Internal Comms fault on the S811+?

Does the S811+ produce Harmonics?

What amount of clearance do I need to have around the S801+ / S811+ soft starters?

Will Eaton soft starters produce harmonics on the lines?

Fault code 46 for S801+

Will a soft start be damaged due to pump back spin?

What is a Service Factor (S.F.)?

Can the keypad be door-mounted on enclosed soft starters?

What CPT or Control Power Transformer should I use with the S611 soft starter?

Should I use fast or slow blow fuses with a Soft starter?

S801+ and S811+ internal fan operation

Does the S811+ have ABS certification?

S811+ stop from the DIM

Single phase soft starters for 115/240V?

What is F00 in an S611?

Can I run or test an S811+ on the bench?

S811+/S801+ Power Supplies

I get a FC59 on my S811+, but the SCR's check good.

DS7 Accessories & Replacement Parts

DS7 Soft Controller Selection

What does the obsolete S752 soft starter cross to?

how do I return my S811+ back to factory settings?

Where can I get the S611 and S811+ soft starter user manuals?

What is the largest S811+ with Inside-the-Delta Mains configurationi?

Can I use an S811+ or S611 with a phase converter?

How do I select a S811+ soft starter?

S801+ / S811+ Soft Starter Documentation

What are the differences between an S811+ and an S811?

Can the S811+ soft starter communicate a warning status and still change the trip contacts?

Why is the current reading on the S811 so off?

SoftStarter S811+ Lug Kits

What is the accuracy of the S811+ Digital Interface Module

What is be the control and power cable size and length for a S811 RVSS ?

how to apply Power factor capacitor with soft starter

looking for IL to mount User inteface device on my S811 soft starter

do we have a cable replacement for EMA69B DIM remote mounting kit

Can I get the key pad mounted on the door of the enclosure with a S611 soft starter ?

Does the S811+ or S801+ conform to IEC overload trip curves?

What tools are needed for making the connections to the S811+ lugs?

S811+ Upload Error Message PRM DNid

Can IP20 protection be used to eliminate power pole contamination?

What control voltage is available with enclosed soft starters?

What communcation protocols are supported with enclosed S611 soft starters?

What are the keypad options for enclosed soft starters?

Can the keypad be door-mounted on enclosed soft starters?

Are IP20 kits available for the S811+?

Do have a Installation pub for the Dim door mounted kits EMA69x

Do enclosed S611 soft starters have the pumping option?

I need support for my Westinghouse Easy-Start Soft starters.

Do I need to order lugs for my S801 / S811 soft starter?

Where can I find documentation of the DS7 Soft Start Controllers?

Is there a replacment available for an S801T?

How many lugs come in an S611 lug kit?

Should I be grounding my negative power on the PSG power supplies that I'm using with the S811+ soft starters?

Can I use a SmartWire DS7 like a normal unit?

Why is the S811+ /S811 stuck in LCD DIM Menu?

Is there a brake for the S811+?

Can the DS7 be configured for SIL3?

Is there sample connection drawing for an S811+ SIL3?

Are S811+ soft starters SIL3?

What does the Network 2 parameter do in the S811+?

What are soft stop options on the S811+?

A200 300/5 rationCurrent transformer data.

Are the S801+ and S811+ soft starters China roHS 15 approved?

Do the S801+/S811+ soft starters work for Corner Grounded Delta systems?

EU Declaration of Conformity for S810+ and S811+ Soft Starters

Are there CAD files available for the DS7?

Can I disable FC13 on an S811+?

Does the S811+ have an E-Stop?

Why won't the S811+ I replaced for an S801+ start?

FC46 on an S811+

Why does the DIM on an S811+ go dark during starting?

Are parts available for the C514DN0C soft starter?

What is the operating temperature for S801+ / S811+ soft starters ?

what is the power factor of S801 soft starter?

What is the +24V output on the S611 used for?

How much power can I draw from the L-tap terminal on the S611?

How do I program the S811+ Relay Custom Configuration

Is an Isolation contactor required for the S811+?

Are the Internal Bypass contactors in the S811+ fully rated?