Eaton Logo

What is the CH Spa Panel used for

Eaton’s CH Spa Panels are premium factory-assembled “combination” units that provide ground fault protection, as well as a convenient way to turn spa pumps on and off. The NEC requires that all pool and spa pumps be protected by a ground fault interrupter and a disconnect switch mounted within 10 feet of the tub or the spa.

Features
● Two extra circuits for
additional loads
● Limited lifetime warranty
● UL Listed
● Tough powder-coated
galvanized steel enclosure
● Factory-installed
two-pole ground fault
circuit interrupter (GFCI)