Are the BRCAF breakers being replaced?
The BRCAF115 (15A), BRCAF115CS (15A), BRCAF120 (20A) and BRACF120CS (20A) will be replaced with the BRN115AF (15A) and BRN120AF (20A). These are not plug-on neutral types, they have the standard pigtail for the neutral. There is also a higher AIC (22 kAIC) option, BRHN115AF and BRHN120AF available.