Eaton Logo

Can a single phase transformer be used on a three phase source?

Yes.  Any single phase transformer can be used on a three phase source by connecting the primary terminals of the single phase transformer to any two wires of the three phase system.  It does not matter whether the three phase source is three phase three-wire or three phase four-wire.  The input of the transformer will be single phase.