Eaton Logo

What should be the Wire size for the EGS & EGSU type of ATS ?

Power Wiring :

For the wiring of the power side of the ATS, please see the table 2 below :

Machine generated alternative text: Table 2. Wire Sizes for ATSs.Transfer SwitchCoatactor WireNumber ol CablesAmp RatingSize Rangeper Phase400750 kanil -2400300kcniI-1/02

Control Wiring :

For the wiring of the control section of the ATS, all the sensors which can be wired with their step wise procedure a diagram can be found in the attached IL for the EGS & EGSU type ATS.

  1. Green ATS EGSU400NSEAC _ EGS400NSE Instruction Manual.pdf