Eaton Logo

Identify date code for load centers

The Lincoln Plant Date Code Policy is in the following format: F # # # &.

 

  • The “F” is the code for the Lincoln, IL plant.
  • The next three digits indicate the year and week of manufacture.
  • The “&” sign at the end signifies the decade of the 2000’s

 

 

Therefore, the date code F251& would indicate that the product was manufactured in the 51st week of 2002. The decade symbols are represented below.

Decade of 1980 – 1989        +

Decade of 1990 – 1999        =

Decade of 2000 – 2009        &

Decade of 2010 – 2019         !

Decade of 2020 – 2029        @

Decade of 2030 – 2039        #

Decade of 2040 – 2049        $