What Breakers to use in a BR load center where the bus is without the notch ?
According to the sample Publication for such panels it uses the duplex/quadplex breaker without the rejection tab, so the notches would not be applicable. It lists BR and BRD not BD or BQ breakers. Attached is a copy of the PUB with the breaker types indicated with a red outline.
So, in order to put up the breaker in this bus without notch, the breakers without rejection tab will be used like the ones shown below :
for more information please see non - CTL type of breakers in the attached catalog : Vol1_Tab1.