Eaton Logo

Sleeve for the breaker lugs in load centers as new code...

There is lug kit to cover up the terminals as shown below :

 

This is just for example…

This sleeve was added in order to comply with New UL67 standards for panel boards and other residential products. These sleeves are also available as separate kit for the lugs, the part number of the sleeves can be seen in the attached launch announcement letter, the letter also consists of basic information of the UL67 requirement and the sleeves.

  1. OneLaunch_announcement_letter_UL67_Finger_Safe_Non_CTL.pdf