What are the torque values for ground bar kits?
The torque values apply to the following catalog numbers:
GBK5
GBK520
GBK1020
GBK1420
GBK10
GBK21
GBK14
Torque for Wire Pressure Screws
#14-10 AWG | 20 lbs*in |
#8 AWG | 25 lbs*in |
#6-8 AWG | 35 lbs*in |
#3-2/0 | 50 lbs*in |
Please see the attachment for official documentation.