Eaton Logo

How to determine if my circuit is suitable for use with an arc fault breaker?

The arc fault circuit breaker is suitable for use with all 1 and 2 pole (15 and 20 amp) residential circuits where a conventional breaker might be used. An arc fault breaker is suitable for detecting rupture in the insulation of the wire where current might jump across (have an arc fault) that could lead to potential hazard.