Eaton Logo

Will this meter breaker unit accept BJ type breakers?

If the meter breaker has two rows of breakers then the BJ breaker would fit.  The two pole BJ breaker requires four spaces, two on each side of the bus.  If the meter stack has a single stack of breakers, then the BJ breakers will not fit in the meter breaker.  See attached drawing for visual reference.

  1. Meterbreaker compatibility with BJ breaker.pdf