Eaton Logo

Surge Products

What is the difference between Type 1 and Type 2 Surge Protective Devices?

What is the difference between the CHSPT2 Series ULTRA and SURGE models?

Can a CHSPT1-208Y be connected directly to the main breaker?

Do I need to register a CHSPT Surge product for warranty purposes?

Does Eaton Surge Breaker provide surge protection for all circuits in the panel or just the one connected to the breaker?

What is the best location to place a surge device in the panel ?

Do you have loadcenters that come with surge products installed?

Is there such a thing as surge breakers?

Does Eaton's type 2 whole home surge devices require a dedicated breaker?

can i add further cable to pigtail in my SPD?

What Type 1 Surge Product (installed before or after main device) Does Eaton offer for Residential/light commercial applications

Does Eaton offer Surge protection for Three-Phase 120/208 Wye

Where do I send my CHSPT2ULTRA for warranty repair?

Do surge units (CHSP) need to be registered upon purchase or installation?

Where can I find information on whole house surge protection?

What the lowest value or smallest surge the CHSPT1ULTRA would pick up?

Does Eaton Offer Coaxial Surge Protection

Where can I find installation instructions for Type 1 Surge Protection Device

What are the differences for UL 1449 3rd edition for surge protection

Do we have installation instructions for CH surge devices

What is the part number for the flush mount kit for a CHSPT2ULTRA?

What residential surge device does Eaton offer that can be used on 3 phase applications?

Does Eaton still make the CHSPTELE?

How long are the wire leads on Resi Surge Device?

Will the CHSA surge device cover my connected equipment?

Can you use a Type 2 whole home surge device on a three phase system?