Eaton Logo

Can safety switch lugs be changed in the field to allow larger wire?

Eaton's safety switches can not have alternative lugs installed in the field. Enclosures for the safety switches are designed to be space efficient with the maximum wire bending radius of the standard lug sizes in mind. If the lugs are changed to accommodate larger wire size, the maximum wire bending radius could be exceeded using the standard enclosure. For alternative lug solutions contact the Eaton Flex Center in Cleveland TN for availability. The Flex Center can be reached by calling 888-329-9272 option 1, option 2 or flexswitches@eaton.com .