Eaton Logo

What generators are compatible with EGSX automatic transfer switches?

Type EGSX transfer switches are only compatible with current Eaton or Generac generators (air cooled or liquid cooled 60kw and below). EGSX transfer switches do not have a control board and rely on the generator for all sensing. The switch requires a 12vDC output from the generator in order transfer power. If this can not be provided from the generator the switch will not work properly.