Eaton Logo

How do I install a GFCI breaker in a Residential Loadcenter?

After installing the breaker, connect the pigtail to the neutral bar, and both the load and neutral wires to the breaker in the positions indicated. In 2 pole 240vac applications it is not necessary to return a neutral to the breaker if you have no load neutral. The pigtail must be connected to the neutral bar in order for the breaker to provide ground fault protection.