Eaton Logo

What kind of locking device can I use on a CHB breaker?

Answer as of 02/19/206

The CHB breaker is a CH breaker in a special cradle that allows the breaker to be turned into a bolt-in breaker. So the CHB breaker will use the same accessories as a standard CH breaker. For example a handle lock use part # CHLO which is a lock dog or CHPL which is a pad lockable device.