Eaton Logo

Can I use a Ground Fault breaker without a neutral?

A neutral must be present in the panel for the ground fault breaker pigtail to be attached to, as the ground fault sensor requires this to be properly powered. With single pole ground fault breakers, you will need a neutral from the load side as well. Two pole ground fault breakers can operate without a neutral from the load.