Eaton Logo

Can I replace the lugs on a CC & CCV Residential Breaker?

YES you can replace a damaged lug on a CC or CCV residential Circuit breaker. But you must know the amperage of the breaker before ordering a new lug. The lug is the same size on Line or Load.

For CC or CCV breakers: 100 up to 150amp use part # TC150CC -- wire size that the lug will accept: #6 up to 4/0

For CC or CCV breakers: 175 up to 200amp use part # CCL300 --- wire size that the lug will accept: 2/0 up to 300mcm

Please note the lugs are packaged one each, so you will have to order a quantity of 2 or 4.